Are there any resources showing how to connect a single DDR3 to an SC594?
I've looked at the ADSP-SC584 EZ-Board schematic and it shows a DDR2 connection. It shows in-line resistors on all the interface lines.
I've looked at the ADSP-SC594 Evaluation Board (EV-SC594-SOM) schematic (as I'm looking at using that part on something else too) and that doesn't have in-line resistors, it has pull-up or are they biasing resistors to VTT (1/2 DDR VDD)?
Can someone please explain why the difference between the two?
How should I connect a DD3 to the SC584?
Thanks,
GGG