I am using the 10/100/1000 emac of sc589 to transfer data, but I can not found any routine about the emac, so I can not start.
Who has the 10/100/1000 emac routine on sc589, if you have, could you share it with me. I appreciate it
Best wishes!
I am using the 10/100/1000 emac of sc589 to transfer data, but I can not found any routine about the emac, so I can not start.
Who has the 10/100/1000 emac routine on sc589, if you have, could you share it with me. I appreciate it
Best wishes!
Hi,
This issue is already handled through private support. To avoid duplication of efforts, please continue the discussions there.
Regards,
Anand Selvaraj.
Thank you for contacting Analog Device's Processor Support.
Could you please explain more about "emac routine" that you are looking for?
However, you can refer the example code "ethernet_test.c" available in ADSP SC-589 Board Support Package. We would suggest you to download and install the ADSP-SC589 Board support package in the below mentioned link.
http://download.analog.com/tools/EZBoards/SC5xx/Releases/Release_2.0.2/ADI_ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2.exe
Once you install the BSP package, the "ethernet_test.c code can be fund from the below installation path
[Installation Directory]\Analog Devices\ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2\ADSP-SC5xx_EZ-KIT\Examples\Power_On_Self_Test\common\source
We would also suggest you to refer the (Page No.2092) for more information on "Ethernet Media Access Controller (EMAC)" in ADSP-SC58x Hardware Reference Manual. Please find the link in below,
https://www.analog.com/media/en/dsp-documentation/processor-manuals/SC58x-2158x-hrm.pdf
Regards,
Processor Application Support.
Hi, some time ago has been busy with other things, this network debugging put a period of time. Following the instructions you gave me, I tested the Ethernet _ test.c code file.
The development board used is the official sc589 development board.
The project used is: [Installation Directory] \ Analog Devices \ ADSP-SC5xx _ EZ-Kit _ Lite-Rel2.0.2 \ ADSP-SC5xx _ EZ-Kit \ Examples \ Power _ On _ Self _ Test.
I use the network cable to connect the 100 MB network port of the development board to the computer, and then run the program. the result is as follow:
Clocks CGU0 (MHz): CCLK-450 SCLK-225 SCLK0-112 SCLK1-112 DDRCLK-450 OCLK-150
Update the CGU0 Setting to supply 125Mhz to EMAC0
Clocks (MHz): CCLK-375 SCLK-187 SCLK0-93 SCLK1-93 DDRCLK-375 OCLK-125
Testing EMAC0
Waiting for the link to be established
So the link is not established, I do not know why, If I should configer my computer or install some software? Could you help me to give me the direction to go forward.
Thanks
Best wishes
who can help me, I'll give him paid help. This is my email: 86675289@qq.com ,
Hi,
We are checking on this case we will get back to you ASAP.
Meanwhile, Can you please let us know your CCES version ? It will be appreciated if you could test the code in CCES 2.9.3 and update us.
Regards,
Anand Selvaraj.