Dear All
where can I find Device Programer for ADSP-21573?
I have tried to use the one form SC573 (sc573_w25q128fv_dpia_Core1.dxe) but the flashing stacks without error.
sc573_w25q128fv_dpia_Core1.dxe
Thanks in advance
Goran
Hi,The sc573_w25q128fv_dpia_Core1.dxe is the DPIA that can be used to communicate with the flash device for ADSP-SC5XX sharc processors. Please let me know if you are facing any issue on communicating the flash device or in booting the flash.However, i would suggest you refer the Readme_W25Q128FV_DPIA.html file available in ADSP-SC5xx Board Support Package. It helps to step through the procedure to implement the interface between the CrossCore Embedded Studio (CCES) Command-Line Device Programmer (CLDP) utility and the on-board device.Please find the link in below to download the ADSP-SC5XX Board Support Packagedownload.analog.com/tools/EZBoards/SC5xx/Releases/Release_2.0.2/ADI_ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2.exeRegards,Anand Selvaraj.
Is there a Device programmer for ASDP-21573?
Hi,Please note that the Device Programmer Interface Application (DPIA) can be used for ADSP-21573 that available in ADSP-SC5XX Board Support Package.Please find the device driver and check with readme file in the below path .C:\Analog Devices\ADSP-SC5xx_EZ-KIT_Lite-Rel2.0.2\ADSP-SC5xx_EZ-KIT\Examples\Device_Programmer\sc573\sharcRegards,Anand Selvaraj.
Thanks