ADSP-21589 DMA SGU clocking config?

So I set CGU like so ...

CGU0_CTL 00001200

CGU0_DIV 04894241

By my reckoning, that configuration is:


SYS_CLKIN 25MHz
CGU_CTL: DF = 0
CGU_CTL: MSEL = 18     PLLCLK = (SYS_CLKIN / (DF+1)) * MSEL (25MHz / 1) * 18 = 450MHz
CGU_DIV: OSEL = 18     OCLK = (SYS_CLKIN / (DF+1)) * MSEL / OSEL (25MHz / 1) * 18 / 18 = 25MHz
CGU_DIV: DSEL = 9     DCLK = (SYS_CLKIN / (DF+1)) * MSEL / DSEL (25MHz / 1) * 18 / 9 = 50MHz
CGU_DIV: S1SEL = 2     SCLK1 = SYS_CLKIN / S1SEL (25MHz / 2) = 12.5MHz
CGU_DIV: SYSSEL = 2     SYSCLK = (SYS_CLKIN / (DF+1)) * MSEL / SYSSEL (25MHz / 1) * 20 / 2 = 225MHz
CGU_DIV: S0SEL = 2     SCLK0 = SYS_CLKIN / S0SEL (25MHz / 2) = 12.5MHz
CGU_DIV: CSEL = 1     CCLK = (SYS_CLKIN / (DF+1)) * MSEL / CSEL (25MHz / 1) * 20 / 1 = 450MHz

In the HRM Introduction section, DMA is "Clocked by SCLK0 from CGU0 and SCLK1 from CGU1". In my configuration, SCLK0 is set to 12.5MHZ, is that the limit? I am trying to stream audio data from RAM to SPORT: 32 bits wide word * 2 * 384K. It works flawless at 192K, starts corrupting at 384K. Do I need a different clock configuration to set the DMA clock higher?

Parents Reply Children
  • Thanks for the reply. Yes it is a typo, we are using ADSP-21584. The datasheet answers my question, we are setting SCLK0 too low. I think we will have to use CGU0 and CGU1 to get all the clocks we need.

  • I made a mistake in the calculation of SCLK0 and SCLK1. With the correction, the DMA blocks are already getting fast clocks, and therefore, still have the original problem that 384K audio is corrupting, 192K is not.

    SYS_CLKIN			25MHz
    CGU0_CTL: DF = 0:	Pass SYS_CLKIN to PLL		
    CGU0_CTL: MSEL = 18:	PLLCLK = (SYS_CLKIN / (DF+1)) * MSEL=	(25MHz / 1) * 18=	450MHz
    CGU0_DIV: CSEL = 1:	CCLK = PLLCLK / CSEL=	450MHz / 1=	450MHz
    CGU0_DIV: OSEL = 18:	OUTCLK = PLLCLK / OSEL=	450MHz / 18=	25MHz
    CGU0_DIV: DSEL = 9:	DCLK = PLLCLK / DSEL=	450MHz / 9=	50MHz
    CGU0_DIV: SYSSEL = 2:	SYSCLK = PLLCLK / SYSSEL=	450MHz / 2=	225MHz
    CGU0_DIV: S1SEL = 2:	SCLK1 = SYSCLK / S1SEL=	225MHz / 2=	112.5MHz
    CGU0_DIV: S0SEL = 2:	SCLK0 = SYSCLK / S0SEL=	225MHz / 2=	112.5MHz
    

  • 0
    •  Analog Employees 
    on Feb 21, 2019 12:38 PM over 1 year ago in reply to misterdsp

    Hello,

    It seems you are working on Audio processing where the SPORT peripheral is used to transmit the sampled data in your custom board.

    However, I also like to know the more information about your end application and the issue which you are facing now?

    Please confirm whether the issue is present on debugging time (or) booting time ?

    Regarding the issue, It would be helpful if you could share us the minimal project which would replicate the issue in ADSP-SC58x EZkit.

    Regards,
    Lalitha