Post Go back to editing

ADSP-21571 SPI Slave Boot problem

Hi,

I'm trying to boot an ADSP-21571 using SPI Slave mode, but I just can't get it to work.
I'm pretty sure I have configured my SPI Master correctly (msb-first, pos. clk polarity). At the moment I'm running at a very low rate (1MHz).

When analyzing the Boot Stream (as generated by the elfloader tool), I can not quite understand the value of Target Address field in the Block Headers.
From what I understand, for a Normal Block, the Target Address should always be the byte address of where the payload should be loaded.
However, all Target Address fields have $28 in the most-significant byte. The other 24 bits seem to represent the correct address, but multiplied with a factor 2,4, 12 etc compared to the address found in the generated map-file.

Could someone please shed some light on this?

By the way, are there any examples on how to boot an ADSP-.21571 in SPI Slave mode available?

Thanks!

Parents
  • Hi Anderson,

    I understand that SPI slave boot is not working for ADSP-21571. Is this correct? Can you please check the below and see if this could be of help.

    Can you please let me know how are you loading the .ldr file and sending it from the Host processor?
    Note that the SPI slave boot types do not need bit reversing necessarily. For SPI slave boots to non-PROM devices, the same default exists (bit-reversed); however, the host can simply be configured to transmit LSB first. Are you doing so?

    Please ensure that the correct boot kernel is used before generating the loader (.LDR) file. If you are using a modified boot kernel, try using the default boot kernel supplied with CCES together with a simple LED blink code to confirm basic boot-loading.

    Also, ensure that you have selected the correct parameters while generating the .LDR file. Selecting an inappropriate parameter may cause the boot to fail. Please choose the loader option (Boot mode (-b)) as ‘SPI slave’ for booting from the external host processor.

    Meanwhile I would suggest you to try booting a simple LED blink application and check if that boots correctly. BTW, is it possible for you to hook up the SPI signals from the host and check if the data is sent out correctly?

    Regards,
    Lalitha S

  • May I have your answer that what is the boot kernel?

Reply Children