Article How can I boot an ADSP-21584 based SHARC application?

By default, CCES provides the ARM based init code. For booting ADSP-21584 based SHARC applications, SHARC init code may be required. Attaching an example init code which can be modified as per the system requirements (CGU/DMC settings). Make sure that the following steps are taken care while generating the loader file:

1. Select the SHARC init code executable as shown in the following screenshot.

2. Select the ADSP-21584 dxes as shown in the below screenshot.

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.