Article ADSP-SC58x/2158x SPI - Example Code

The attached code is used for data transfer using SPI peripheral. Any of the SPI instances can be used as master or slave with each SPI being a Tx or Rx. There are macros to select between the various configuration options. The same code can used for core mode or DMA mode data transfer.

SPI_MasterTx_Slave_Rx_Core1.zip

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.