The MLB clock signal is available as part of the pin mux. Pin PD14 when configured with the MUX configured as “10” will route the MLB clock on this pin which can be used for external connections.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
The MLB clock signal is available as part of the pin mux. Pin PD14 when configured with the MUX configured as “10” will route the MLB clock on this pin which can be used for external connections.