Article Does the user have option to decide between F1 Active mode and E2 Active mode in Hardware Counter based Loops?

Determination of F1-active or E2-active mode for a hardware counter based loop is based on the opcode.

Loops not having a change of flow (jump, call etc.) or IDLE in last eleven instructions of the loop body are safe to execute as F1-active mode. The assembler identifies loops which are safe to execute in F1-active mode and uses the F1- active opcode.

Short loops with few iterations where the total number of instructions of fully unrolled loop is less than eleven, always execute as E2-active mode irrespective opcode.

 

But the user can force all the counter based loops to execute in E2-Active mode by setting the SLOWLOOP bit [bit 7] of MODE2 register (Note that this bit is intended to be primarily used by the debugger).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.