The MLB clock signal is available as part of the pin mux. Pin PD14 when configured with the MUX configured as “10” will route the MLB clock on this pin which can be used for external connections.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
The MLB clock signal is available as part of the pin mux. Pin PD14 when configured with the MUX configured as “10” will route the MLB clock on this pin which can be used for external connections.