ADSP-SC58x: FAQ

  • ADSP-SC584 SPORT Core mode example

    Attached is the example code for SPORT I2S mode with an external PCG trigger, designed for the ADSP-SC584 utilizing Core mode. ADSP-SC58x_SPORT_CoreMode.zip
  • ADSP-SC58x example code for firmware upgrade via UART

    Attached is the ADSP-SC58x example code for firmware upgrade via UART along with multiple loader streams. Also the attached ADSP-SC58x_UART_Firmware_Upgrade.pdf document contains the procedure to upgrade…
  • ADSP-SC58x FMU(Fault Management Unit) Example Code.

    Attached is an example project for the FMU in SC58x family. This gives an example of how fault sources and fault responses can be configured. The Macros in the code allow to choose any one of the various…
  • ADSP-SC58X How to configure EMDMA Gather mode

    The purpose of scatter/gather DMA is the transfer of data from/to non-contiguous memory blocks. The scatter/gather DMA type is a fixed block size scatter/gather DMA that relies on tap list entries in system…
  • ADSP-SC58x Multicore SPORT TDM example

    Attached are the ADSP-SC58x example codes for SPORT TDM mode. These codes are configured to transfer data between two cores using internal clock/FS and external clock/FS in different sampling rate(48KHz…
  • ADSP-SC58x SPI Quad example code

    Attached is the code examples0 for SPI Quad Master Transmit/Receive and Slave Receive/Transmit which is tested across two ADSP-SC584 Ez-Kit. SPI_Quad.zip
  • ADSP-SC58x/2158x ACM- Example code

    Attached code configures ACM to acquire samples from an ADC via SPORT0 interface. The ACM can be triggered via three sources and this particular example uses external trigger which can be changed for other…
  • ADSP-SC58x/2158x ASRC:Example codes

    Attached are the example codes for ASRC of ADSP-SC58x/2158x processors. Please find the information about each attachement below, 1. SRC configured in I2S mode 2. SRCs configured in TDM mode: 8 ASRCs…
  • ADSP-SC58x/2158x Cortex A5 Software Interrupt- Example code

    Attached code shows how to trigger software interrupt from Cortex A5 core to same core. This code runs in Cortex A5 in ADSP-SC58x processor. Software_Interrupt_Core0.zip
  • ADSP-SC58x/2158x Counter: Example code

    Attached is the sample code of Counter for ADSP-SC58x processors. Counter_Binary_mode.zip

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.