Hi there,
I'm looking for an IC that can simultaneously:
- Encode 2-4 audio channels of 48Khz, 16-bit, 2.5ms frames, using lc3plus.
- Decode and mix 8-12 audio channels of 48Khz, 16-bit, 2.5ms frames, using lc3plus.
1. Can you recommend such a chip? (If the ADSP-SC598 is an overkill, which one can do this cost-effectively?)
2. Is lc3plus easily supported as a pre-compiled library, or as a "block" in a visual design tool? I'm ok with C/C++ programming as/if needed.
3. Is there built-in support for UAC2 over USB if I want to connect the system to a DAW / digital mixer?
4. I already have an ADAU1777 in my current design. Would you recommend leaving the ADAU1777 in place as a Front-End audio processor and connect it to the MCU/DSP over I2S, or do the amps on the proposed chip match or exceed those of the ADAU1777, in which case I can remove the ADAU1777 from the design?
Thanks in advance,
Nir