ADSP-21565 ICT TEST FAIL , if the DSP is suitable for ICT test


KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
ADSP-21565
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21565 on Analog.com
ADSP-21565 ICT TEST FAIL , if the DSP is suitable for ICT test


Hi Danieli,
We are checking with our internal team and we will get back to you as soon as possible.
Regards,
Nandini C
Hi Nandini ,
please check ,thanks!
During PCB manufacturing, we performed ICT (In-Circuit Test) on boards assembled with ADSP-21565 devices.
On some I/O pins, low-current ICT tests (diode, resistance-to-GND, and capacitance) showed abnormal readings, such as lower-than-expected diode or resistance values, or abnormal capacitance results.
An ABA test was performed by replacing the ADSP-21565 device on the same board. After replacement, the previously observed abnormal capacitance behavior was no longer present, indicating variation between devices under identical ICT conditions.
ICT performed using low-current VI / IDT methods
Device unpowered or only biased by the ICT system
Same fixture and test program used
We understand that ADSP-21565 is a high-complexity DSP with internal structures such as input buffers, programmable pull-ups/pull-downs, and JTAG / boundary-scan logic, which may affect low-current ICT measurements.
We would appreciate ADI’s guidance on the following:
Whether ICT diode, resistance, or capacitance tests are suitable for PCBA-level testing of ADSP-21565 I/O pins
Whether ADI recommends alternative or preferred test methods for ADSP-21565 at the PCBA level (e.g., boundary scan, functional test, or limited ICT coverage)
Any official recommendations to avoid false failures during production testing
Hi Nandini ,
may I know the process for the update ? thanks
Hi Danieli,
We are currently checking with our internal team and we will get back to you as soon as possible.
Regards,
Nandini C
Hi Nandini ,
would you please push again ?