Post Go back to editing

ADSP-21565 ICT TEST

Category: Datasheet/Specs
Product Number: ADSP-21565

ADSP-21565 ICT TEST  FAIL , if the DSP is suitable for ICT test

 

  • Hi Danieli,

    We are checking with our internal team and we will get back to you as soon as possible.

    Regards,
    Nandini C

  • Hi Danieli,
    Please find the below response from our internal team.
    >>> Can you please explain what is ICT in detail?
    Regards,
    Nandini C
  • Hi Nandini  ,

     please check ,thanks!

    During PCB manufacturing, we performed ICT (In-Circuit Test) on boards assembled with ADSP-21565 devices.

    Observed Behavior

    On some I/O pins, low-current ICT tests (diode, resistance-to-GND, and capacitance) showed abnormal readings, such as lower-than-expected diode or resistance values, or abnormal capacitance results.

    An ABA test was performed by replacing the ADSP-21565 device on the same board. After replacement, the previously observed abnormal capacitance behavior was no longer present, indicating variation between devices under identical ICT conditions.

    Test Conditions

    • ICT performed using low-current VI / IDT methods

    • Device unpowered or only biased by the ICT system

    • Same fixture and test program used

    Request for ADI Confirmation

    We understand that ADSP-21565 is a high-complexity DSP with internal structures such as input buffers, programmable pull-ups/pull-downs, and JTAG / boundary-scan logic, which may affect low-current ICT measurements.

    We would appreciate ADI’s guidance on the following:

    1. Whether ICT diode, resistance, or capacitance tests are suitable for PCBA-level testing of ADSP-21565 I/O pins

    2. Whether ADI recommends alternative or preferred test methods for ADSP-21565 at the PCBA level (e.g., boundary scan, functional test, or limited ICT coverage)

    3. Any official recommendations to avoid false failures during production testing

  • Hi Nandini  ,

    may I know the process for the update ? thanks

  • Hi Danieli,

    We are currently checking with our internal team and we will get back to you as soon as possible.

    Regards,
    Nandini C

  • Hi Nandini  ,

    would you please push again ?

  • Hi,
    Please find the below response from our internal team,
    1.Whether ICT diode, resistance, or capacitance tests are suitable for PCBA-level testing of ADSP-21565 I/O pins
    >>>ICT testing at PCB level is more complex than just testing DSP. So, not sure if it will yield consistent results. For example, the only testing done during manufacturing of DSP eval boards are continuity tests of the traces during PCB FAB, and POST (Power-On-Self-Test) of the assembled boards.
    2.Whether ADI recommends alternative or preferred test methods for ADSP-21565 at the PCBA level (e.g., boundary scan, functional test, or limited ICT coverage)
    >>>The Production test by ADI of ADSP-21565W includes boundary scan, functional test, ICT testing, etc. at Automotive temperature range (-40 to 125C). The customer could test their application across temperatures. They could also develop unit tests for their board based on POST example from EV-21569-SOM BSP, and run across temperatures
    >>>When performing ICT testing, the customer has to make sure to follow the Absolute Maximum Ratings specified in the datasheet. For example, when powered-off, the voltage input to the I/O pins should be between ±0.2V
    >>>The Absolute Maximum Ratings of all pins should also be followed when DSP signals are interfaced outside the PCB (for example, UART pins connected to external Serial port)
    3.Any official recommendations to avoid false failures during production testing
    >>>During ADI production testing, pins are tested if they are open or short but not for specific impedance.  There is no specification for resistance on a pin, and customer cannot assume defective part due to inconsistencies between parts.
    Regards,
    Nandini C

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.