Post Go back to editing

DSP

Thread Summary

The user inquires about creating a PROM boot file for the ADSP-21060 using VisualDSP++5.1.2 and an Atmel AT27C010. The final answer confirms that the AT27C010 is an OTP EPROM and cannot be programmed using the DSP, suggesting the use of an external EPROM programmer instead.
AI Generated Content
Category: Software
Product Number: ADSP-21060L
Software Version: VisualDSP++5.1.2

How to use VisualDSP++5.1.2 make ADSP-21060 PROM boot file.

I use Atmel AT27C010 as boot PROM,the schematic look pic.

thank you very much.

my email: yonghengyz@outlook.com

  • Hi,

    Are you asking about the file which is used to program the Atmel AT27C010. Could you please confirm.

    We understand that Atmel AT27C010 is one-time programmable, read-only memory (OTP EPROM). So, the EPROM can't be programmed using the DSP and therefore there is no driver file available for the same. One way to program the EPROM could be to use external EPROM programmer (or universal programmer) sort of kits.

    Regards,
    Nandini C

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.