Is ADSP-21569 capable of multi-threading coding?
I wonder that ADSP-21569-SOM has multi-thread function.
So I would like to run two tasks for the interrupt function that occurs whenever a mic. wave sample detects.
Is this possible?
ADSP-21569
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21569 on Analog.com
Is ADSP-21569 capable of multi-threading coding?
I wonder that ADSP-21569-SOM has multi-thread function.
So I would like to run two tasks for the interrupt function that occurs whenever a mic. wave sample detects.
Is this possible?
Hi,
The ADSP-21569 processor supports FreeRTOS, which provides the capability for multitasking.
This FreeRTOS can be integrated into your project using the available add-in. Please refer to the links below for more detailed information.
https://www.analog.com/en/resources/evaluation-hardware-and-software/embedded-development-software/…
https://wiki.analog.com/resources/tools-software/freertos
If this is not meet your requirement, please explain your query in detail.
Waiting for your reply.
Regards,
Nandini C
Thanks for your reply.
^_^ ADI chip has lots of amazing functions!
Thanks for your reply.
^_^ ADI chip has lots of amazing functions!