Hi,
I am using 21835-SOM board.I found that the serial port cannot communicate properly.
Please help me check the code.
Regards,UARTDMAMode.rar
Bingo
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADSP-21835
Recommended for New Designs
The ADSP-2183x/ADSP-SC83x digital signal processors (DSPs)
are members of the SHARC®-FX family of products. The
SHARC-FX core uses a single-instruction...
Datasheet
ADSP-21835 on Analog.com
Hi,
I am using 21835-SOM board.I found that the serial port cannot communicate properly.
Please help me check the code.
Regards,UARTDMAMode.rar
Bingo
Hi Bingo,
Could you please provide more information about the exact issue you are facing, so we can assist you more effectively?
Additionally, please confirm whether the example provided in the ADSP-SC8xx BSP is working as expected.
Regards,
Nandini C
Hi,
My code only uses uart0 and connected to PC via USBC,have the processor return the received data.But the processor did not return any data.
I only have adsp21835w-ev-som board,so I can not verify UART project in ADSP-SC8xx BSP.
Regards,
Bingo
Hi,
Could you please tye my code,You can use any UART terminal.
regards,
Bingo
Hi,
Test steps:
1.run the example code first
2.send 8 bytes by UART terminal
UART terminal config:
baudrate:57600
stop bit:1
data bit:8
parity:none
I can not find UART registers:

Core mode screenshot of UART terminal:

DMA mode screenshot of UART terminal:

Regards,
Bingo
Hi Bingo,
Thank you for sharing the information.
Please find the UART register in the Peripherals view, which displays each peripheral and its memory-mapped registers. Please follow the below step to find the Peripherals view.
Window -> Show View -> Other -> Debug -> Peripherals
We tested the code with the configurations you provided, but no output was received. Could you please try using the terminal like Tera Term, putty, etc and let us know if you get the same result.
Please note that there are no data lines available on the P1 connector. The P1 connector is used solely to power the ADSP-21835 SOM board. Please find the below schematic for reference.

We understand that you do not have the EV-SOMCRR-EZKIT and EV-SOMCRR-BRKOUT boards along with the ADSP-21835-SOM board. Please confirm.

Regards,
Nandini C
Hi,
1.I do not have the EV-SOMCRR-EZKIT and EV-SOMCRR-BRKOUT.
2.there is a USB to UART chip on ADSP-21835 SOM board,please check you USB cable.

3.echo received by putty,uart in core mode

4. register view of core mode

5.register view of DMA mode

6.no echo in DMA mode,but receiving Interrupt happened.

Hi Bingo,
We are checking this internally and will get back to you as soon as possible.
Regards,
Nandini C
Hi,
May I ask if there has been any progress?
Regards,
Bingo
Hi,
Apologies for the delay caused.
We were able to simulate your issue on our end; we are checking and will get back to you as soon as possible.
Regards,
Nandini C
Hi,
Please refer the attached example demonstrates the usage of baud rate detection automatically using “UART DMA” mode to scan the keyboard alphabets and send them onto a Terminal emulator such as TeraTerm.UART_DMA_Autobaud_SC835_SHARCFX_Core1.zip
Please open a serial terminal application (for example PuTTY or TeraTerm) and configure a serial connection to the COM port with the settings as shown below:
Bits Per second = Set any baud rate, range between 110 to 115200 bps
Data bits = 8
Parity = None
Stop bits = 1
Flow Control = None
And follow the below steps:
1. Open a terminal emulating tool such as tera term on PC and set the baud rate at which communication needs to be established.
2. Run the example and enter "@" in the terminal emulator window so that the example can detect the baud rate and it will be displayed on the console window as "Detected Baudrate is xx"
3. Any key pressed through keyboard will be displayed on the console window and to exit from this program press "Enter".
Please run this example and let us know if any assistance is required.
Regards,
Nandini C
Hi,
Why must the receive buffer be placed in the L1 RAM?Does this have to do with the cache settings?
Where can the cache settings be modified?
Regards,
Bingo
Hi,
Why must the receive buffer be placed in the L1 RAM?Does this have to do with the cache settings?
Where can the cache settings be modified?
Regards,
Bingo
Hi Bingo,
Please find the attached example code where the buffer is placed in L2 memory. Please ensure that the cache management API is properly configured and the buffers are aligned to cache line boundaries when the cache is enabled.
6012.UART_DMA_Autobaud_SC835_SHARCFX_Core1.zip
The ADI_CACHE_MANAGEMENT macro defined in the "adi_pdma_config_SC8xx.h" file enables/disables cache management by the driver.
Aligning buffer memory to cache line boundaries ensures that cache maintenance operations apply to the buffer memory alone, and not operate on unrelated data that may inadvertently share memory space on that cache line. This may not be an issue for most applications, but it can cause problems if adjoining, misaligned memory is also being accessed or written off-core, possibly by DMA or by another processor core.
Regarding "Where can the cache settings be modified?"
>> In order to configure cacheable and non-cacheable ranges, or otherwise change the cacheability settings of specific regions of memory, use the Startup Code/LSP Add-in to configure the cache settings for each memory segment. The settings are accessed by double-clicking on a memory segment to edit it, then clicking the Edit button next to "Access Properties" to change the MPU settings for the segment.
For more information, please refer the below CCES help path.
CrossCore® Embedded Studio 3.0.1 > SHARC®-FX Development Tools Documentation > CrossCore Embedded Studio SHARC+ to SHARC-FX Migration Guide > Configuring cache settings on SHARC-FX
Regards,
Nandini C