Post Go back to editing

ADSP-SC59X USB Interface - File Transfer from USB to SD Card

Category: Hardware
Product Number: ADSP-SC598

Hello,

Question: 

  1. If a micro SD is connected using the eMSI interface, is it possible to read/write files stored on a micro SD through the USB interface on the SC598?
  2. Is a USB PHY required for this kind of file transfer?

Details:

  • I want to use the ADSP-SC598 for an audio based product. I will use the eMSI to interface with a micro SD card.
  • I would like to connect a PC to the SC598 through a USB cable to be able to transfer files between the PC and the micro SD. Is this scenario possible?
  • I am new to USB functionality and have limited knowledge on what is possible / required.
  • I plan to purchase the evaluation modules to verify the various peripherals, but wanted to know specifically about the USB.

Best regards,

Dimitri