Hi
Is it possible to use the OSPI interface on the SC598 to stream data to an external device?
I would like to stream logging data over QSPI. The stream of data will not be continuous or constant data rate.
Best Regards
Howard
ADSP-SC598
Pre release
Reaching speeds of up to 1 GHz, the ADSP-SC598/SC596/SC595 processors are members of the ADSP-SC59x SHARC® family of products. Containing the same dual...
Datasheet
ADSP-SC598 on Analog.com
Hi
Is it possible to use the OSPI interface on the SC598 to stream data to an external device?
I would like to stream logging data over QSPI. The stream of data will not be continuous or constant data rate.
Best Regards
Howard
Hi Howard,
Is it possible to use the OSPI interface on the SC598 to stream data to an external device?
>>> Yes, You can use the Octal SPI in SC598.
You can refer the SOMCRR-EZKIT and SC598 SOM schematics for OSPI interface.
Also, Please refer the "ospi" examples available in Board support package of SC59x for programming purposes.
download.analog.com/.../ADI_EV-SC59x_EZ-KIT-Rel3.2.0.exe
After installation please navigate as below.
<Installation path>:\Analog Devices\EV-SC59x_EZ-KIT-Rel3.2.0\EV-SC59x_EZ-KIT\Examples\drivers\ospi
Let us know for further assistance.
Regards,
Ranjitha R
Hi
I looked at the BSP and the hardware reference manual for the SC59x and they only seem to talk about interfacing the OSPI to Flash chips.
I want to use it for sending data to an external data logger for sending high speed data to a PC for analysis.
Hi
Do you have an update on this please
Hi Howard,
Sorry for the delay.
If Data Logger has support for OSPI, by referring to the flash interfacing in schematics you can interface the logger. You can also refer the maximum speed supported for OSPI
In the "Table 22. Clock Operating Conditions " Pg: 62 of SC598 Datasheet. https://www.analog.com/media/en/technical-documentation/data-sheets/adsp-sc596-adsp-sc598.pdf
Also, You can try configuring the device with taking the BSP example as reference as per your application.
Regards,
Ranjitha.R
Hi
I've been trying to get SPI DMA working, based on the example in "EV-SC59x_EZ-KIT-Rel3.2.0" , but the DMA seems to terminate early, resulting in missing data.
I've recreated the issue with a simple test program in the attached zip. When I run the program, it should be sending 12 bytes to SPI-1, but only 10 bytes are being sent. I've attached screen grab of the DSP trace.
The program configures the following GPIO for SPI output
/* Configure PA_10 as SPI1_CLK */
/* Configure PA_11 as SPI1_MISO */
/* Configure PA_12 as SPI1_MOSI */
/* Configure PA_13 as SPI1_SEL1 */
It initiates a 12 byte DMA transfer, then waits 100ms before initiating another.
Why is the DMA not sending 12 bytes as I expect?
Best Regards
Howard
spi_dma_test.zip
Hi Howard,
Apologies for the delay in getting back to you.
The ENUM_DMA_CFG_XCNT_INT bit generates a DMA interrupt based on the Xcount value.
If this interrupt occurs after the specified number of transfers, it might lead to data loss. So the SPI buffer hasn't yet received all the data on the buffer. We suggest you to using the ENUM_DMA_CFG_PERIPH_INT instead of ENUM_DMA_CFG_XCNT_INT.
This configuration has been tested on the SC594 SOM Board and successfully sent 12 bytes. Please test this configuration on your setup and let me know the outcome.
Regards,
Nandini C