Hello,
I want to program this Ic:ADSP -21469 KBCZ-4 but i don’t know how to program this IC. Please guide me how to program this IC and which programmer and software do i need to program this IC?
ADSP-21469
Production
The fourth generation of SHARC® Processors, which includes the ADSP-21469, offers increased performance, hardware-based filter accelerators, audio and...
Datasheet
ADSP-21469 on Analog.com
ADSP-21479
Production
The fourth generation of SHARC® Processors now includes the low power floating point DSP products – the ADSP-21478 and ADSP-21479 and offers increased...
Datasheet
ADSP-21479 on Analog.com
Hello,
I want to program this Ic:ADSP -21469 KBCZ-4 but i don’t know how to program this IC. Please guide me how to program this IC and which programmer and software do i need to program this IC?
Hi,
You can use VisualDSP++ or CCES to program the ADSP-21479.We recommend CCES IDE which is the eclipse-based IDE for the Analog Devices Blackfin®, SHARC® and Arm® processor families. Employing the latest generation of our mature code generations tools, this Eclipse based IDE provides seamless, intuitive C/C++ and assembly language editing, code-gen, and debug support. Please let us know which tool you are preferring to program.
Refer the below product page of both tools.
CCES: www.analog.com/.../adswt-cces.html
VisualDSP++: www.analog.com/.../vdsp-bf-sh-ts.html
Also are you asking to Developing the application, debug, and program(load) the .ldr file or only for programming.
Regards,
Divya.P
While repairing a motherboard, I accidentally damaged this IC, causing a bulge at the center during reballing. Now, I need to create an exact copy of this IC. Can you guide me on which programmer to use for copying this IC?
Hi,
Could you please share us below details to assist you better.
1. Now, I need to create an exact copy of this IC. Can you guide me on which programmer to use for copying this IC? >> What do you mean by Exact copy of this IC. Please explain your query in detail.
2. When processor comes out of reset, based on Boot mode it loads the program. Let us know which boot mode are you using ? Please refer “Table 8. Boot Mode Selection” in the below linked datasheet:
www.analog.com/.../ADSP-21467_21469.pdf
3. Are you have .ldr file to program? if so, which tool are you used before to generate loader file.
Regards,
Divya.P
I have the software and require the IC(ADSP-21469) along with the corresponding programmer for its programming, utilizing the 8-pin JTAG interface. Could you please advise me on the appropriate programmer required for this task?
Hi,
You can use ICE-1000/2000 and VDSP/CCES tool to program. Please refer the below link:
www.analog.com/.../emulators.html
Please contact your nearest ADI sales and distributors to buy ADSP-21469 processor. Please find the link given below.
www.analog.com/.../find-sale-office-distributor.html
Follow the below steps If you are using VDSP:
Refer readme file available in the below link and go through “V. USING LOADER FILES” for complete procedure
C:\Program Files (x86)\Analog Devices\VisualDSP 5.1.2\214xx\Examples\ADSP-21469 EZ-Board\Power_On_Self_Test
Follow the below steps If you are using CCES:
Please install Board support package from the below link
download.analog.com/.../ADI_ADSP-21469_EZKIT-Rel1.0.0.exe
After installation, please refer readme file available in the below link and go through “5. Using Loader Files” for complete procedure
Please refer below to install CCES or VDSP:
For VisualdSP++ :
Here is the doanload link to get the latest VisualDSP++ 5.1.2.
download.analog.com/.../VisualDSP 5.1.2.exe
Test Drive license is available to download free of charge from our website. This license entitles you to 90 days of Simulator and Emulator sessions before the license expires.
You can register for a Test Drive license on our website here:
form.analog.com/.../visualDSPTestDrive.aspx
For CCES:
You can download and install latest version of CCES 2.12.0 from the below link:
download.analog.com/.../ADI_CrossCoreEmbeddedStudio-Rel2.12.0.exe
An evaluation license can be obtained from CrossCore Embedded Studio,which offers a tool chain evaluation license the first time it runs. It can be activated once on a particular machine for 90 days.
Please refer the below FAQ to obtain evaluation license for CCES
FAQ: How can I obtain and install a license for CrossCore Embedded Studio?
ez.analog.com/.../faq-how-can-i-obtain-and-install-a-licenses-for-crosscore-embedded-studio
Regards,
Divya.P
Hello
I have Atmel-ICE, can I use this one, or do I need to use ICE-1000/2000?
Hi,
You have to use ICE-1000/2000 emulator to connect with ADSP-21469 processor.
www.analog.com/.../emulators.html
ICE-1000 is low-cost emulator which has two connectors used for connecting to a target. J1 is a 0.1" 14-pin connector used for interfacing with legacy targets(ADSP-21469). 10-pin connector used on newer processors.
Please refer the below link for details:
ez.analog.com/.../introducing-the-adzs-ice-1000-and-adzs-ice-2000-emulators
Regards,
Divya.P