Post Go back to editing

How to use CANFD on Industrial Grade (-40oC – +125oC) ADSP-SC596/SC598 Models?

Category: Datasheet/Specs
Product Number: ADSP-SC596; ADSP-SC598

How to use CANFD on Industrial Grade (-40oC – +125oC) ADSP-SC596/SC598 Models?

  • In order to use the CANFD on Industrial-grade ADSP-SC596/SC598 models, please make sure to use the CCES project session with the ‘W’ suffix, as highlighted in the screenshot below.

     

    This will enable the project to make use of CANFD drivers in the project development, which are not available for sessions without the ‘W’ suffix. This will also ensure that the appropriate preload code is executed to initialize the CANFD memory, which is needed to allow debugger access to the CANFD memory and registers.