How to use CANFD on Industrial Grade (-40oC – +125oC) ADSP-SC592/SC594 Models?
ADSP-SC594
Production
Reaching speeds of up to 1 GHz, the ADSP-SC59x processors are members of the SHARC® family of products. The ADSP-SC59x processor is a dual-SHARC+® core...
Datasheet
ADSP-SC594 on Analog.com
How to use CANFD on Industrial Grade (-40oC – +125oC) ADSP-SC592/SC594 Models?
In order to use the CANFD on Industrial-grade ADSP-SC592/SC594 models, please make sure to use the CCES project session with the ‘W’ suffix, as highlighted in the screenshot below.
This will enable the project to make use of CANFD drivers in the project development, which are not available for sessions without the ‘W’ suffix. This will also ensure that the appropriate preload code is executed to initialize the CANFD memory, which is needed to allow debugger access to the CANFD memory and registers.