As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...
Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...
This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...
This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...
Can SPI memory mapped mode be used for write access?
Only read accesses are supported in memory-mapped mode.
For programming the flash with instructions or for writing raw data, non memory-memory mapped mode must be used.