What are the new modes that are introduced in Link Port for ADSP-SC59x?
What are the new modes that are introduced in Link Port for ADSP-SC59x?
The conventional Link Port mode is 8 bit mode which is Single data rate
New modes that have been introduced are:
4-bit Single data rate - uses D0,D1,D2,D3 data pins
2-bit Single data rate - uses D0,D1 data pins
4-bit Double data rate - uses D0,D1,D2,D3 data pins
2-bit Double data rate - uses D0,D1 data pins
In Double data rate data is sampled both on rising and falling edge