Post Go back to editing

Boot Mode to be used to program the external flash

Category: Hardware
Product Number: ADSP-21566

I am using the EV-21569-SOM and an ICE-2000 emulator for programming.

My goal is to program the external flash using the emulator and then boot the DSP from the external flash.

Do we need to keep the DSP in No Boot/Custom Boot mode (BMODE[2:0] = 000) while programming the external flash using the ICE-2000 emulator, and then change BMODE to 001 for booting from the external flash?

Could you please confirm if this is the recommended procedure?

Thread Notes

  • Hi,

    Regarding "Do we need to keep the DSP in No Boot/Custom Boot mode (BMODE[2:0] = 000) while programming the external flash using the ICE-2000 emulator, and then change BMODE to 001 for booting from the external flash?"
    >>>Yes, Your understanding is correct. it is recommended to set BMODE =0 (No Boot) when flashing an LDR file on the EV-21569-SOM. Once flash programming is completed, change BMODE[2:0] = 001 (SPI Master Boot) to boot the application from the external SPI flash.

    Could you please follow the "Creating/Using Loader File" and "Flashing the Loader file" section in the "Readme_21569_SOM_POST.html". Please download and install the ADSP-2156x BSP from the below link.
    download.analog.com/.../ADI_EV-2156x_EZ-KIT-Rel3.0.0.exe

    Once installed, the POST Readme can be available in the below path.
    [Installation directory]:\Analog Devices\EV-2156x_EZ-KIT-Rel3.0.0\EV-2156x_EZ-KIT\Examples\Power_On_Self_Test\Readme\21569\Readme_21569_SOM_POST.html

    Regards,
    Nandini C

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.