| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. Met after 17 hours |
Awaiting Company Response | |
ADSP-21565
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21565 on Analog.com
"I'm designing a board around the ADSP-21565 with three power rails — 3.3V (ADP7104), 1.8V (AP2112K), and 1.1V (TPS62130A). The 1.8V feeds VDD_REF and VDD_ANA, the 1.1V feeds VDD_INT, and 3.3V feeds VDD_EXT. Does the ADSP-21565 have any hard power sequencing requirements between these rails, and if so, does a passive RC-based sequencing approach satisfy them or is active sequencing required?"
regards,
Mark.
Hi, Nandini, and thank you for your reply.
Could you possibly point me to a reference design or application note that shows the recommended active sequencing approach for the ADSP-21565 with 1.1V, 1.8V, and 3.3V rails? Specifically whether a dedicated sequencing IC is recommended or whether a simpler RC and enable pin approach is sufficient.
regards,
Mark.
Hi,
This query has been handled via the following support ticket ID: CS-578559-R5N1N7
We have shared a detailed response with you through our private support channel regarding the recommended power sequencing approach for the ADSP-21565.
To avoid the duplication of efforts, please continue the discussion there.
Regards,
Nandini C
Thank you, Nandidi.
regards,
Mark.
Thank you, Nandidi.
regards,
Mark.