We have board designs that support both ADSP-21569 and ADSP-21593. This means we have sufficient core supply for the 21593.
I understand that the ADSP-21835 is almost pin compatible. We boot from an external SPI flash and this has changed.
Can the ADI team outline the changes that are needed to do one or both of the following:
1. Changes needed to make an existing hardware design universal.
2. If this is impractical, then a complete list of changes needed.
I am sure many other users have this question and no one wants to do two revisions if they miss something the first time.
Al