Post Go back to editing

ADSP-21568 SOM and EV-SOMCRR-EZLITE POST User Input

Thread Summary

The user encountered issues selecting a test number on the ADSP-21568 SOM and EV-SOMCRR-EZLITE board using the keyboard and buttons. The solution was to use the sequence CTRL+J instead of the ENTER key in Tera Term to select commands or test numbers.
AI Generated Content
Category: Hardware
Product Number: EV-21568-SOM

Hello,

ADSP-21568 SOM and EV-SOMCRR-EZLITE are connected. When I launched the POST project with CCES, the starting log can be printed on the serial terminal as below.

btw, how to select the test number? Both keyboard and PB1/PB2 button on the EV-SOMCRR-EZLITE don't work.

Thanks.

*******************************************************
*** ADSP-21568 SOM and EV-SOMCRR-EZLITE Board Power-On Self Test
*******************************************************
Built on Mar 24 2025, at 10:54:07
Firmware version: 1.0
Clocks (MHz): CCLK-937 SCLK-468 SCLK0-117 SCLK1-234 OCLK-117

Waiting for User Input: Command or a Test number to be selected...