Post Go back to editing

EV-21569-SOM (Rev C) schematics + DSP info

Category: Datasheet/Specs
Product Number: ADSP21569

Hello,

We are currently designing a daughter board using the EV-21569-SOM.
The website currently only provides Rev A schematics, whilst the board we purchased is Rev C, and we noticed several differences.
Would it be possible to get our hands on the newer schematics, and possibly a 3D file of the board to check clearance?

I noticed a thread that had a similar request (https://ez.analog.com/dsp/software-and-development-tools/cces/f/q-a/590542/ev-21569-som-rev-c-and-ev-somcrr-ezkit-rev-d-do-not-work-with-bsp), but the schematics weren't shared publicly.
If you have any other notes or files concerning the changes I would also happily take them, especially since the current BSP apparently does not communicate well with the clock generator, which is a component that we would like to exploit.


While I am at it, I would also like to confirm the maximum SPI slave clock speeds for the ADSP-2156x.
The datasheet mentions f_SPICLKEXT is 62.5 MHz maximum for receiving data with an external clock.
We initially intended to use a 100 MHz clock (from the aforementioned generator) for an ADC to get 8 datapoints per period but we seemingly have to settle with 50 or 62.5 (for 4 or 5 datapoints respectively, which isn't bad either, but more=better).

Best regards,

Arcady Ruvidic

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.