KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
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
ADSP-21569
Recommended for New Designs
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21569 on Analog.com
Back for the second episode of my series.
I have therefore expanded the project code illustrated in the first post of this series (here: SPI slave mode shifting 1s on MISO pin during adi_spi_DMARead() operation - Q&A - ADSP-2156x - EngineerZone) to get one step closer to the real-world application I'm going to develop.
In my application idea, master SPI is going to transfer N bytes to the slave, then slave SPI is going to transfer M bytes back to the master, all in a single transaction (by transaction I mean that, from SPI masters' point of view, the whole data exchange would be equivalent to a single transfer of N+M bytes).
To simulate this new scenario, I then applied the following changes to the code:

<--- in SPIDMAMode.h, replacing DESC_BUFFER_SIZE macro
<--- in SPIDMAMode.c


<--- new callback code
<--- changes in main() to pass SPI handlers as callback parameters.
Keeping SPI clock to around 1.3 MHz as in my previous post the result is exactly as expected:

but later when trying to raise clock frequency just a little bit to around 1.6MHz, this is what starts to happen:

clearly meaning that adi_spi_DMAWrite() inside Callback() is taking too long while disabling/enabling SPI slave peripheral.
This is what emerges by "looping the SPI dance forever" then analyzing the situation with statistical profiling:

So, the question is: how can I improve this behavior? There's no solution other than stop using ADI SPI driver and switching to a lower-level approach?
Thanks in advance to anyone who wants to contribute
Hello again,
by forcing READY line low as the first instruction in Callback() code and forcing it high again as the last instruction in Callback() code, I verified that the overall execution time of Callback() does not take (relatively) that long, but that the most expensive part of the whole DMA mode switching operation resides in the interrupt latency!

As you can see in the image above, I measured around 1us delay starting from CLK rising edge during last bit in the last SPI master transmitted byte and ending when READY line is brought low by Callback() invocation. 1us latency looks to be way too much.
Hello again,
by forcing READY line low as the first instruction in Callback() code and forcing it high again as the last instruction in Callback() code, I verified that the overall execution time of Callback() does not take (relatively) that long, but that the most expensive part of the whole DMA mode switching operation resides in the interrupt latency!

As you can see in the image above, I measured around 1us delay starting from CLK rising edge during last bit in the last SPI master transmitted byte and ending when READY line is brought low by Callback() invocation. 1us latency looks to be way too much.