Dear,
I'm designing an ANC case with ADSP-21565 and AD1939. I want to know the definition of DAI pins that it can tell me which pin is ABCLK, ALRCLK, DBCLK, DLRCLK and so on.
I would be very grateful if you could help me.
Best Regards.
Zhip
AD1939
Production
The AD1939 is a high performance, single-chip codec that provides four analog-to-digital converters (ADCs) with differential input, and eight digital-to...
Datasheet
AD1939 on Analog.com
ADSP-21565
Production
Reaching speeds of up to 1 GHz, the ADSP-2156x processors are members of the SHARC® family of products. The ADSP-2156x processor is based on the SHARC...
Datasheet
ADSP-21565 on Analog.com
Dear,
I'm designing an ANC case with ADSP-21565 and AD1939. I want to know the definition of DAI pins that it can tell me which pin is ABCLK, ALRCLK, DBCLK, DLRCLK and so on.
I would be very grateful if you could help me.
Best Regards.
Zhip
Dear Nandini.C,
Thank you very much for your reply. Your understanding is correct. Following your advice, I have reviewed the relevant documents about "Digital Audio Interface (DAI)" and "Signal Routing Units (SRUs)". However, I find it difficult to understand for me. Could you please help me check the following connections which are referenced in the schematic "EV-21562-AUTO"?
| ADSP-21565 | AD1939 | |
| DAI0_PIN03 | → | DBCLK |
| DAI0_PIN04 | → | DLRCLK |
| DAI0_PIN08 | → | DSDATA1 |
| DAI0_PIN07 | → | DSDATA2 |
| DAI0_PIN06 | → | DSDATA3 |
| DAI0_PIN05 | → | DSDATA4 |
| DAI0_PIN20 | → | ABCLK |
| DAI0_PIN19 | → | ALRCLK |
| DAI0_PIN09 | → | ASDATA1 |
| DAI0_PIN10 | → | ASDATA2 |
Hi Zhip,
While looking into the connection table you have shared, the Hardware connections between the ADSP-21565 and AD1939 seems correct.
Please let us know if you require further assistance, along with additional details.
Regards,
Nandini C
Thank you a lot for your help.