Hi.
While I developed my software I found some errors in HRM version 0.7. Some errors were issued by me early.
1. The chapter Link ports has many errors. So I recommend to use ADSP-2159x/ADSP-SC592/SC594 HRM revision 0.7.
2. The field "Description/Enumeration" of the 12-58: PADS_PORT[n]_PDE Register Fields have wrong text: "Pull-Up Disable". The right text must be "Pull-Down Enable".
3. The sub-chapter Core Driven Memory Transfer Compute-and-Compare Mode on page 1414 have wrong text in point of number 6:
Initialize the CRC_CTL register with the CRC_CTL.OPMODE bit set to memory scan compute-and-compare mode and the CRC_CTL.BLKEN bit configured to enable the CRC peripheral.
The right text is
Initialize the CRC_CTL register with the CRC_CTL.OPMODE bit set to memory transfer compute-and-compare mode and the CRC_CTL.BLKEN bit configured to enable the CRC peripheral.
Best regards.