Post Go back to editing

Clarification on calculating SPDIF_TX_HFCLK_I clock speed required for 192KHz SPDIF transmission

Category: Hardware
Product Number: ADSP-21569

I'm trying to work out the correct clock configuration required to transmit SPDIF at 192KHz.

Looking at the example SPDIF loopback program, am I right in thinking that SPDIF_TX_HFCLK_I  needs to be 4x SPDIF_TX_CLK_I?

Therefore, am I right in thinking that the absolute clock speeds required for the SPDIF clock inputs to transmit at 192KHz would be:

SPDIF_TX_CLK_I = 12.288MHz

SPDIF_TX_FS_I = 192KHz

SPDIF_TX_HFCLK_I = 49.152MHz



typo
[edited by: MichaelF91 at 9:30 AM (GMT -4) on 15 May 2024]