Post Go back to editing

Not restart after soft reset

Category: Hardware
Product Number: ADSP-21565
Software Version: 2.11.0.0

Hi.

I want to do a soft reset because the signal sometimes becomes abnormal.

I wrote adi_rcu_ControlSystemReset(0,true);, so it returns to the start address but cannot restart.

What should I do?

Thanks & Best Regards,

YAMAMOTO

Parents
  • Hi Yamamoto,

    Can you please refer the RCU example code available in the ADSP-21569 Board support package. Please download and install the ADSP-21569 BSP from the link given below.
    download.analog.com/.../ADI_EV-2156x_EZ-KIT-Rel1.0.1.exe

    Once installed, you can find the RCU examples and the Readme file from the below mentioned installation path.
    [Installation directory]:\Analog Devices\EV-2156x_EZ-KIT-Rel1.0.1\EV-2156x_EZ-KIT\Examples\services\rcu

    Please use the code as a reference and modify as per your requirement.

    Regards,
    Ranjitha R

Reply
  • Hi Yamamoto,

    Can you please refer the RCU example code available in the ADSP-21569 Board support package. Please download and install the ADSP-21569 BSP from the link given below.
    download.analog.com/.../ADI_EV-2156x_EZ-KIT-Rel1.0.1.exe

    Once installed, you can find the RCU examples and the Readme file from the below mentioned installation path.
    [Installation directory]:\Analog Devices\EV-2156x_EZ-KIT-Rel1.0.1\EV-2156x_EZ-KIT\Examples\services\rcu

    Please use the code as a reference and modify as per your requirement.

    Regards,
    Ranjitha R

Children