Post Go back to editing

Not restart after soft reset

Category: Hardware
Product Number: ADSP-21565
Software Version: 2.11.0.0

Hi.

I want to do a soft reset because the signal sometimes becomes abnormal.

I wrote adi_rcu_ControlSystemReset(0,true);, so it returns to the start address but cannot restart.

What should I do?

Thanks & Best Regards,

YAMAMOTO

  • Hi Yamamoto,

    Can you please refer the RCU example code available in the ADSP-21569 Board support package. Please download and install the ADSP-21569 BSP from the link given below.
    download.analog.com/.../ADI_EV-2156x_EZ-KIT-Rel1.0.1.exe

    Once installed, you can find the RCU examples and the Readme file from the below mentioned installation path.
    [Installation directory]:\Analog Devices\EV-2156x_EZ-KIT-Rel1.0.1\EV-2156x_EZ-KIT\Examples\services\rcu

    Please use the code as a reference and modify as per your requirement.

    Regards,
    Ranjitha R

  • Thank you Ranji.

    I tried but it stopped at the start address and I could not restart.


    I set adi_rcu_ClearBCodeReg(0,ADI_RCU_BCODE_REG_HALT);

    If it detects a lockout. adi_rcu_ControlSystemReset(0, true);.

    Please tell me how to do this.

    I want to do a soft reset and restart from the start address when the digital input signal is lost in an audio product.

    How should I describe this?

    Please tell me.
    Please.

    Thanks & Best Regards,

    YAMAMOTO

  • Hi Yamamoto,

    To assist you better on this, can you please provide more information on below points.
    1) Can you please confirm whether your application is working in debug time.
    2) Is the flashed application working as expected during Hardware reset?
    3) What boot mode you are using? Did you change the boot mode during soft reset?

    Regards,
    Ranjitha R

  • Hi.

    It didn't work in debugging, but it did work after a reset on the actual device.
    It still does not work the way I want it to.
    Please let me know if you need to ask any questions.
    Thank you very much.

    Regards,

    YAMAMOTO

  • Hi Yamamoto,

    Can you please share the simple project to replicate the issue in ADSP-21569 Ez-kit, so that we can assist you better on this.

    Regards,
    Ranjitha.R

  • Hi.

    Thanks.

    I would like to consider the response after running it on the actual machine, so I will think about it me.

    Thanks & Best Regards,

    YAMAMOTO