Post Go back to editing

Is HADC/TMU supported in ADSP-2156x products?

Thread Summary

The user inquired about HADC/TMU support in ADSP-2156x processors. The final answer confirms that HADC and TMU are not supported in ADSP-21566/21567/21569 processors due to reliability risks. However, an accompanying answer suggests that these features are now supported, though this conflicts with the latest silicon anomaly list, which states HADC is not functional for Rev. 0.0 of the 21569. The user's 21569KBCZ10 samples (datecodes 2118, 2202, 2237) are Rev. 0.0, and HADC functionality is not guaranteed. The datecode for Rev. 0.2 of the 21569KBCZ10 is pending confirmation.
AI Generated Content

I do not see the HADC/TMU reference in the datasheet and hardware reference manual for ADSP-2156x processor. Is this supported or not?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.