Post Go back to editing

Secure Boot Loader stream generation

Thread Summary

The user asked how to generate secure loader streams in Blp, Blx, and Blw formats. The final answer provided the signtool utility from CCES, including sample commands for generating Blp and Blw streams, and noted that the tool supports generating ECDSA key pairs and encryption keys. For detailed options, the help command is recommended.
AI Generated Content

How to generate secure loader stream in the formats Blp, Blx and Blw?

Edit Notes

tagged content
[edited by: JValeriani at 7:26 PM (GMT 0) on 3 Sep 2019]
Parents
  • CCES provides signtool utility to generate secure boot streams in formats Blp, Blx or Blw. A sample command to do the same is given here. The same tool has options to generate the ECDSA key pair and the encryption keys.

    Generation of Blp boot loader stream:

    "<CCES installation path>\signtool.exe" sign -type BLp -attribute 0x80000002=<BCODE value> -attribute 0x80000003=<give 256 or 224 here based on the EDCSA type> -prikey <ecdsa keypair.der>  -infile <input loader stream file to be signed> -outfile <output file path>

    Generation of Blw boot loader stream

    "<CCES installation path>\signtool.exe" sign -type BLw -prikey <ecdsa keypair.der> -infile <input loader stream file to be signed> -enckey <encryption key.bin> -wrapkey <wrapkey.bin> -outfile <output file path>

     For a complete list of the options supported by this tool, use the help option as below

    "<CCES installation path>\signtool.exe" -help

Reply
  • CCES provides signtool utility to generate secure boot streams in formats Blp, Blx or Blw. A sample command to do the same is given here. The same tool has options to generate the ECDSA key pair and the encryption keys.

    Generation of Blp boot loader stream:

    "<CCES installation path>\signtool.exe" sign -type BLp -attribute 0x80000002=<BCODE value> -attribute 0x80000003=<give 256 or 224 here based on the EDCSA type> -prikey <ecdsa keypair.der>  -infile <input loader stream file to be signed> -outfile <output file path>

    Generation of Blw boot loader stream

    "<CCES installation path>\signtool.exe" sign -type BLw -prikey <ecdsa keypair.der> -infile <input loader stream file to be signed> -enckey <encryption key.bin> -wrapkey <wrapkey.bin> -outfile <output file path>

     For a complete list of the options supported by this tool, use the help option as below

    "<CCES installation path>\signtool.exe" -help

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.