When accessing the SPI flash with more than 128Mb *ldr,it is recommended to change byte addressing from 3 byte to 4 byte in flash.To access the memory array beyond 128Mb.This can be done by Entering the…
Attached "DDR Sweep Test code" for ADSP-SC594 which is performed for different types of accesses (e.g., core, DMA, 8/16/32/64-bit) and different data patterns (for example, all 0x0, all 0xF, all 0x5, all…
Yes, to use the 450MHz part for any frequency, the SVSnominal method need to be used. The Static Voltage Scaling (SVS) is an alternate voltage specification technique that can provide significant performance…
Yes, ASRC TDM mode uses the opposite clock edge for sampling and driving the inputs and outputs when compared to modes. Please note that the information which is provided in the datasheet under "Asynchronous…
BLp:
"<CCES Root Directory>\signtool.exe"-add-sbh-hash-224 or 256 sign -type BLp -prikey "path of auth_key.bin file" -infile "path of input loader stream file to be signed " -outfile "give path, where…
Multi-rate filters change the sampling rate of a signal—they convert the input samples of a signal to a different set of data that represents the same signal sampled at a different rate. Decimation: A…
An SSL is a stand-alone application that is executed at boot time before the actual application is dynamically loaded into memory. The SSL can be used to invoke a ROM API to boot a second application.…
Using SPI slave mode boot, the processor consumes boot data from an external SPI host device. Please find the attached SPI slave booting code for ADSP-21489 processor. This code can be tested across two…
Please refer the attached project which configures the FMU to issue a system reset on the event of WDOG expiry. Keep the BMODE as 1 before running the code.
Once the WDOG expired, system reset happens…