This webinar will introduce remote-controlled edge nodes and how they promise to simplify the automotive network architecture and expedite the integration...
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
      1. Quote of the week: "Knowledge is knowing a tomato is a fruit. Wisdom is not putting it in a fruit salad" - unknown Sources: commons.wikimedia...

    View All

    What's Brewing

      GMSL Quiz! Read the blog, take the quiz, and enter to win a gift card!

      Quiz! Read the GMSL Link Lock Blog - Take the Quiz and You are Entered to Win! Important: Read the blog first . The quiz questions are all based on...
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
    The Limitation of Heat Dissipation IO-Link is used across many branches of factory automation, and in these applications, areas of the factory floor...

     

    GMSL Debugging: Getting a Lock

    Imagine a scenario where you have a brand-new board design or are excited to try out some evaluation kits only to find out that the two devices can’t talk...
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
Other ADI Processors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other ADI Processors
  • Processors and DSP
Other ADI Processors
Documents Does the onewire SDK ver410 API support TMLine function?
  • Q&A
  • Files
  • Docs
  • Members
  • Tags
  • More
  • Cancel
  • Documents
  • About Other ADI Processors
  • Can I reserve a block of serial number IDs in the one-wire products?
  • +DS1822Z+: FAQ
  • +DS1825U+: FAQ
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20: FAQ
  • +DS18S20: FAQ
  • +DS2401+: FAQ
  • +DS2401A+: FAQ
  • +DS2401P+: FAQ
  • +DS2430A+: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • DS2431Q+T&R: FAQ
  • DS2432 Replacement
  • DS2432P+T&R: FAQ
  • +DS2465P+: FAQ
  • +DS2475R+T: FAQ
  • -DS2480B+: FAQ
    • After configuring the POL pin of DS2480B, how long does it take before it comes into effect?
    • After the DS2480B is powered-on, how long before the MCU can communicate with it via the UART interface?
    • Does the DS2480 exhibit eventual undesired states?
    • Does the onewire SDK ver410 API support TMLine function?
    • If the DS2480B receives an unexpected command (e.g., F0) after power-on, would that cause the DS2480B to enter an undefined state and then suspend?
    • The default programming pulse duration of the DS2480B is too short. How do you adjust it?
  • DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484EVKIT#: FAQ
  • +DS2484R+T: FAQ
  • +DS2484R+U: FAQ
  • +DS2488X+T: FAQ
  • +DS24B33+: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS2505: FAQ
  • DS28C36: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28C36Q+U: FAQ
  • +DS28C39: FAQ
  • +DS28C40G/V+T: FAQ
  • +DS28C50EVKIT#: FAQ
  • +DS28CM00: FAQ
  • +DS28E02P-W01+4T: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E05R+T: FAQ
  • +DS28E07+T: FAQ
  • DS28E07: FAQ
  • +DS28E15EVKIT#: FAQ
  • +DS28E15G+T: FAQ
  • +DS28E15G+U: FAQ
  • +DS28E17: FAQ
  • +DS28E17K: FAQ
  • +DS28E17Q+: FAQ
  • +DS28E18Q+T: FAQ
  • +DS28E30: FAQ
  • +DS28E36: FAQ
  • +DS28E38EVKIT#: FAQ
  • +DS28E38Q+T: FAQ
  • +DS28E50Q+U: FAQ
  • DS28E80: FAQ
  • +DS28E80Q+T: FAQ
  • +DS28E83G+T: FAQ
  • +DS28E84AQ+T: FAQ
  • +DS28E84AQ+U: FAQ
  • +DS28E84Q+T: FAQ
  • +DS28EC20+: FAQ
  • DS28EC20: FAQ
  • +DS28EC20P+: FAQ
  • +DS28EL22: FAQ
  • +DS3640: FAQ
  • +DS3644B+: FAQ
  • +DS3645B+: FAQ
  • DS3645B: FAQ
  • +DS3900H2EVKIT#: FAQ
  • +DS9488-GP8#: FAQ
  • Is it possible to expand the storage temperature range of the DS2431P+T&R from 125℃ to 150℃?
  • +MAX31820PARMCR+: FAQ
  • +MAX31826MTA+: FAQ
  • +MAX31826MUA+: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX36011/W+T: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • +MAXQ1061ETP+: FAQ
  • +MAXQ1061EUD+: FAQ
  • We have a set of DS2502 with wrong coding, is it possible to revise them? Is there any way to allow these products to continue to be used?

Does the onewire SDK ver410 API support TMLine function?

No, the latest API does not have any direct support for the TMLine function.  

However, the TMLine calls mentioned in the Application note 4104 under CONFIGURATIONS OF 1-WIRE TIMING OF THE DS2480B can be used to port the code.

Tags: KA-15238 DS2480B+ TMLine OneWire DS2480B