Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Other ADI Processors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other ADI Processors
  • Processors & DSP
Other ADI Processors
Documents How long does it take to read and write to the DS28E84 memories?
  • Q&A
  • Files
  • Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • About Other ADI Processors
  • Can I reserve a block of serial number IDs in the one-wire products?
  • +DS1822Z+: FAQ
  • +DS1825U+: FAQ
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20+T&R: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20: FAQ
  • +DS18S20: FAQ
  • +DS2401+: FAQ
  • +DS2401A+: FAQ
  • +DS2401P+: FAQ
  • +DS2430A+: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • DS2431Q+T&R: FAQ
  • DS2432 Replacement
  • DS2432P+T&R: FAQ
  • +DS2465P+: FAQ
  • +DS2475R+T: FAQ
  • +DS2477: FAQ
  • +DS2480B+: FAQ
  • DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484EVKIT#: FAQ
  • +DS2484R+T: FAQ
  • +DS2484R+U: FAQ
  • +DS2488X+T: FAQ
  • +DS24B33+: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS2505: FAQ
  • DS28C36: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28C36Q+U: FAQ
  • +DS28C39: FAQ
  • +DS28C40G/V+T: FAQ
  • +DS28C50EVKIT#: FAQ
  • +DS28CM00: FAQ
  • +DS28E02P-W01+4T: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E05R+T: FAQ
  • +DS28E07+T: FAQ
  • DS28E07: FAQ
  • +DS28E15EVKIT#: FAQ
  • +DS28E15G+T: FAQ
  • +DS28E15G+U: FAQ
  • +DS28E17: FAQ
  • +DS28E17K: FAQ
  • +DS28E17Q+: FAQ
  • +DS28E18Q+T: FAQ
  • +DS28E30: FAQ
  • +DS28E36: FAQ
  • +DS28E38EVKIT#: FAQ
  • +DS28E38Q+T: FAQ
  • +DS28E50Q+U: FAQ
  • DS28E80: FAQ
  • +DS28E80Q+T: FAQ
  • +DS28E83G+T: FAQ
  • -DS28E84AQ+T: FAQ
    • How long does it take to read and write to the DS28E84 memories?
    • If the PIO pin on the DS28E84 is unused, can it be left unconnected?
    • Is the EPAD electrically connected to IC GND inside the package for the DS28E84?
    • Is the EPAD electrically connected to IC GND on the DS28E84?
  • +DS28E84AQ+U: FAQ
  • +DS28E84Q+T: FAQ
  • +DS28EC20+: FAQ
  • DS28EC20: FAQ
  • +DS28EC20P+: FAQ
  • +DS28EL22: FAQ
  • +DS3640: FAQ
  • +DS3644B+: FAQ
  • +DS3645B+: FAQ
  • DS3645B: FAQ
  • +DS3900H2EVKIT#: FAQ
  • +DS9488-GP8#: FAQ
  • Is it possible to expand the storage temperature range of the DS2431P+T&R from 125℃ to 150℃?
  • +MAX31820PARMCR+: FAQ
  • +MAX31826MTA+: FAQ
  • +MAX31826MUA+: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX36011/W+T: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • +MAXQ1061ETP+: FAQ
  • +MAXQ1061EUD+: FAQ
  • We have a set of DS2502 with wrong coding, is it possible to revise them? Is there any way to allow these products to continue to be used?

How long does it take to read and write to the DS28E84 memories?

This can be found using the combination of the DS28E84 Security User Guide and datasheet. The sequence for a read and write memory are shown in Table 13 and Table 15 of the Security User Guide, while the 1-Wire time by time slot duration, 1-Wire Reset Cycle , and the Strong pullup delay. With this information we can calculate how long the write or read sequence by adding up the total time of each step of the read or write sequence.

For example if the DS28E84 is in Overdrive Speed mode, then from the datasheet:

  • tRSTH = 48us
  • tRSTL = 48us
  • tSLOT = 16us
  • tWM = 100ms

With the example write sequence below:

  1. 1W Reset: tRSTH +tRSTL = 96 us
  2. ROM select: tSLOT x 8 (Skip ROM) = 128us (Byte time)
  3. Length Byte: tSLOT x 8 = 128us
  4. Command: tSLOT x 8 = 128us
  5. Parameter: tSLOT x 8 = 128us
  6. New Page Date: tSLOT * 8 * 32 = 4096us
  7. CRC16: tSLOT * 16 = 256us
  8. Release Byte: tSLOT * 8 =128us
  9. Strong Pullup delay: tWM = 100ms
  10. Dummy Byte: tSLOT * 8 = 128us
  11. Length Byte: tSLOT * 8 = 128us
  12. Result Byte: tSLOT * 8 = 128us
  13. CRC16: tSLOT * 16 = 256us

The fastest write time in overdrive speed mode with the example sequence above would then be the total which is around 105.7ms.

Tags: write time 1-Wire Secure Authenticators time read DS28E84AQ+T read time DS28E84 write KA-14592 1-Wire Devices Show More