Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Other ADI Processors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other ADI Processors
  • Processors & DSP
Other ADI Processors
Documents Why are the commands of Match ROM and Write Memory both 55H in the DS28E05 datasheet? What is the difference between the two?
  • Q&A
  • Files
  • Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • About Other ADI Processors
  • Can I reserve a block of serial number IDs in the one-wire products?
  • +DS1822Z+: FAQ
  • +DS1825U+: FAQ
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20+T&R: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20: FAQ
  • +DS18S20: FAQ
  • +DS2401+: FAQ
  • +DS2401A+: FAQ
  • +DS2401P+: FAQ
  • +DS2430A+: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • DS2431Q+T&R: FAQ
  • DS2432 Replacement
  • DS2432P+T&R: FAQ
  • +DS2465P+: FAQ
  • +DS2475R+T: FAQ
  • +DS2477: FAQ
  • +DS2480B+: FAQ
  • DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484EVKIT#: FAQ
  • +DS2484R+T: FAQ
  • +DS2484R+U: FAQ
  • +DS2488X+T: FAQ
  • +DS24B33+: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS2505: FAQ
  • DS28C36: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28C36Q+U: FAQ
  • +DS28C39: FAQ
  • +DS28C40G/V+T: FAQ
  • +DS28C50EVKIT#: FAQ
  • +DS28CM00: FAQ
  • +DS28E02P-W01+4T: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • -DS28E05R+T: FAQ
    • Does the DS28E05 work with the DS2408 or other standard mode 1-wire devices?
    • How can I maximize the number of writes I can do to the DS28E05?
    • How do I know when I can begin another write command to the DS28E05 EEPROM?
    • There are data written into DS28E05 chip, yet the reading of the written content has failed, meaning the data is not successfully written. What is the cause of this?
    • Where could I find FTDI and Prolific drivers for DS28E05EVKIT 1-wire EEPROM EV kit?
    • Where could I find the "UART 1-Wire Master Utility"?
    • Why are the commands of Match ROM and Write Memory both 55H in the DS28E05 datasheet? What is the difference between the two?
  • +DS28E07+T: FAQ
  • DS28E07: FAQ
  • +DS28E15EVKIT#: FAQ
  • +DS28E15G+T: FAQ
  • +DS28E15G+U: FAQ
  • +DS28E17: FAQ
  • +DS28E17K: FAQ
  • +DS28E17Q+: FAQ
  • +DS28E18Q+T: FAQ
  • +DS28E30: FAQ
  • +DS28E36: FAQ
  • +DS28E38EVKIT#: FAQ
  • +DS28E38Q+T: FAQ
  • +DS28E50Q+U: FAQ
  • DS28E80: FAQ
  • +DS28E80Q+T: FAQ
  • +DS28E83G+T: FAQ
  • +DS28E84AQ+T: FAQ
  • +DS28E84AQ+U: FAQ
  • +DS28E84Q+T: FAQ
  • +DS28EC20+: FAQ
  • DS28EC20: FAQ
  • +DS28EC20P+: FAQ
  • +DS28EL22: FAQ
  • +DS3640: FAQ
  • +DS3644B+: FAQ
  • +DS3645B+: FAQ
  • DS3645B: FAQ
  • +DS3900H2EVKIT#: FAQ
  • +DS9488-GP8#: FAQ
  • Is it possible to expand the storage temperature range of the DS2431P+T&R from 125℃ to 150℃?
  • +MAX31820PARMCR+: FAQ
  • +MAX31826MTA+: FAQ
  • +MAX31826MUA+: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX36011/W+T: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • +MAXQ1061ETP+: FAQ
  • +MAXQ1061EUD+: FAQ
  • We have a set of DS2502 with wrong coding, is it possible to revise them? Is there any way to allow these products to continue to be used?

Why are the commands of Match ROM and Write Memory both 55H in the DS28E05 datasheet? What is the difference between the two?

Match ROM belongs to the ROM Function instruction set. Write Memory belongs to the Memory Function instruction set. These two do not conflict. The sequence of command is:
1. Initialization
2. ROM Function Command
3. Memory Function Command
4. Transaction Data

Tags: 000102678 Match ROM eeprom Other ADI Processors ROM) 1-Wire Memory (EPROM 55h Write Memory DS28E05 1-Wire Devices Show More