Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Other ADI Processors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other ADI Processors
  • Processors & DSP
Other ADI Processors
Documents Why won't the DS28E17K software recognize the USB to 1-Wire Adapter?
  • Q&A
  • Files
  • Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • About Other ADI Processors
  • Can I reserve a block of serial number IDs in the one-wire products?
  • +DS1822Z+: FAQ
  • +DS1825U+: FAQ
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20+T&R: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20: FAQ
  • +DS18S20: FAQ
  • +DS2401+: FAQ
  • +DS2401A+: FAQ
  • +DS2401P+: FAQ
  • +DS2430A+: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • DS2431Q+T&R: FAQ
  • DS2432 Replacement
  • DS2432P+T&R: FAQ
  • +DS2465P+: FAQ
  • +DS2475R+T: FAQ
  • +DS2477: FAQ
  • +DS2480B+: FAQ
  • DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484EVKIT#: FAQ
  • +DS2484R+T: FAQ
  • +DS2484R+U: FAQ
  • +DS2488X+T: FAQ
  • +DS24B33+: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS2505: FAQ
  • DS28C36: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28C36Q+U: FAQ
  • +DS28C39: FAQ
  • +DS28C40G/V+T: FAQ
  • +DS28C50EVKIT#: FAQ
  • +DS28CM00: FAQ
  • +DS28E02P-W01+4T: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E05R+T: FAQ
  • +DS28E07+T: FAQ
  • DS28E07: FAQ
  • +DS28E15EVKIT#: FAQ
  • +DS28E15G+T: FAQ
  • +DS28E15G+U: FAQ
  • +DS28E17: FAQ
  • -DS28E17K: FAQ
    • Why won't the DS28E17K software recognize the USB to 1-Wire Adapter?
  • +DS28E17Q+: FAQ
  • +DS28E18Q+T: FAQ
  • +DS28E30: FAQ
  • +DS28E36: FAQ
  • +DS28E38EVKIT#: FAQ
  • +DS28E38Q+T: FAQ
  • +DS28E50Q+U: FAQ
  • DS28E80: FAQ
  • +DS28E80Q+T: FAQ
  • +DS28E83G+T: FAQ
  • +DS28E84AQ+T: FAQ
  • +DS28E84AQ+U: FAQ
  • +DS28E84Q+T: FAQ
  • +DS28EC20+: FAQ
  • DS28EC20: FAQ
  • +DS28EC20P+: FAQ
  • +DS28EL22: FAQ
  • +DS3640: FAQ
  • +DS3644B+: FAQ
  • +DS3645B+: FAQ
  • DS3645B: FAQ
  • +DS3900H2EVKIT#: FAQ
  • +DS9488-GP8#: FAQ
  • Is it possible to expand the storage temperature range of the DS2431P+T&R from 125℃ to 150℃?
  • +MAX31820PARMCR+: FAQ
  • +MAX31826MTA+: FAQ
  • +MAX31826MUA+: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX36011/W+T: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • +MAXQ1061ETP+: FAQ
  • +MAXQ1061EUD+: FAQ
  • We have a set of DS2502 with wrong coding, is it possible to revise them? Is there any way to allow these products to continue to be used?

Why won't the DS28E17K software recognize the USB to 1-Wire Adapter?

The DS28E17 evaluation software (Ver. 1.3 and earlier) scans COM Ports 0-15 for the adapter. If Windows enumerates the adapter on a COM Port outside of this range, you will need to change the COM Port number for the software to connect to the adapter. If COM0 through COM15 are already in use, you will need to free up one of those ports by switching an existing device to a different port, and then switch the adapter to that newly available port.

To switch the port number of a device, follow these steps:

  1. Open Device Manager as an administrator (Press the Windows key and search "Device Manager," right click "Open Device Manager," and click "Run as administrator.") ​
  2. Expand the Ports (COM & LPT) branch, right click on the device, and select Properties.
  3. Open the Port Settings tab and click Advanced...
  4. Select the new COM Port Number and click OK
Tags: 000100662 DS28E17K