Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Other ADI Processors
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Other ADI Processors
  • Processors & DSP
Other ADI Processors
Documents Can you confirm the DS18S20 is non-magnetic and its function will not be adversely affected by use in an MRI?
  • Q&A
  • Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • About Other ADI Processors
  • Can I reserve a block of serial number IDs in the one-wire products?
  • +DS1822Z+: FAQ
  • +DS1825U+: FAQ
  • DS18B20+: FAQ
  • +DS18B20+PAR: FAQ
  • +DS18B20+T&R: FAQ
  • +DS18B20/GG8: FAQ
  • DS18B20: FAQ
  • -DS18S20: FAQ
    • Can you confirm the DS18S20 is non-magnetic and its function will not be adversely affected by use in an MRI?
    • On the DS18S20, what is the formula for calculating resolutions greater than 9 bits when the temperature is negative?
  • +DS2401+: FAQ
  • +DS2401A+: FAQ
  • +DS2401P+: FAQ
  • +DS2430A+: FAQ
  • +DS2431+: FAQ
  • DS2431P+T&R: FAQ
  • DS2431Q+T&R: FAQ
  • DS2432 Replacement
  • DS2432P+T&R: FAQ
  • +DS2465P+: FAQ
  • +DS2475R+T: FAQ
  • +DS2477: FAQ
  • +DS2480B+: FAQ
  • DS2480B: FAQ
  • +DS2482-100: FAQ
  • DS2484: FAQ
  • +DS2484EVKIT#: FAQ
  • +DS2484R+T: FAQ
  • +DS2484R+U: FAQ
  • +DS2488X+T: FAQ
  • +DS24B33+: FAQ
  • +DS2502+: FAQ
  • +DS2502-E48: FAQ
  • DS2502P+T&R: FAQ
  • +DS2505+: FAQ
  • +DS2505: FAQ
  • DS28C36: FAQ
  • +DS28C36AQ+T: FAQ
  • +DS28C36Q+U: FAQ
  • +DS28C39: FAQ
  • +DS28C40G/V+T: FAQ
  • +DS28C50EVKIT#: FAQ
  • +DS28CM00: FAQ
  • +DS28E02P-W01+4T: FAQ
  • DS28E05: FAQ
  • +DS28E05P+: FAQ
  • +DS28E05R+T: FAQ
  • +DS28E07+T: FAQ
  • DS28E07: FAQ
  • +DS28E15EVKIT#: FAQ
  • +DS28E15G+T: FAQ
  • +DS28E15G+U: FAQ
  • +DS28E17: FAQ
  • +DS28E17K: FAQ
  • +DS28E17Q+: FAQ
  • +DS28E18Q+T: FAQ
  • +DS28E30: FAQ
  • +DS28E36: FAQ
  • +DS28E38EVKIT#: FAQ
  • +DS28E38Q+T: FAQ
  • +DS28E50Q+U: FAQ
  • DS28E80: FAQ
  • +DS28E80Q+T: FAQ
  • +DS28E83G+T: FAQ
  • +DS28E84AQ+T: FAQ
  • +DS28E84AQ+U: FAQ
  • +DS28E84Q+T: FAQ
  • +DS28EC20+: FAQ
  • DS28EC20: FAQ
  • +DS28EC20P+: FAQ
  • +DS28EL22: FAQ
  • +DS3640: FAQ
  • +DS3644B+: FAQ
  • +DS3645B+: FAQ
  • DS3645B: FAQ
  • +DS3900H2EVKIT#: FAQ
  • +DS9488-GP8#: FAQ
  • Is it possible to expand the storage temperature range of the DS2431P+T&R from 125℃ to 150℃?
  • +MAX31820PARMCR+: FAQ
  • +MAX31826MTA+: FAQ
  • +MAX31826MUA+: FAQ
  • +MAX31850EATB+: FAQ
  • +MAX31850KATB+: FAQ
  • +MAX36011/W+T: FAQ
  • +MAX66300-24XEVKIT#: FAQ
  • +MAXQ1061ETP+: FAQ
  • +MAXQ1061EUD+: FAQ
  • We have a set of DS2502 with wrong coding, is it possible to revise them? Is there any way to allow these products to continue to be used?

Can you confirm the DS18S20 is non-magnetic and its function will not be adversely affected by use in an MRI?

Maxim has not tested the performance of the DS18B20 when exposed to high magnetic fields. It is not anticipated that the magnetic field would adversely affect measurements, but Maxim does not have any data to support this claim. As with any critical design metric, Maxim recommends testing circuitry as deemed necessary.  
 
Tags: 1-Wire Temperature Sensors Other ADI Processors DS18S20 DS18B20 000096832 1-Wire Devices Show More