Post Go back to editing

DS2484 behind I2C address translator LTC4317 (double, or single LTC4316)

Thread Summary

The user inquires about using the DS2484 I2C to 1-wire interface with a fixed I2C address alongside the LTC4317 I2C address translator for a multi-segment 1-wire setup. The final answer confirms that this configuration should work fine, with one DS2484 connected directly and the other two via the LTC4317. The DS2482-100 is not an option due to its address selection capabilities.
AI Generated Content
Category: Hardware
Product Number: DS2484
Dear forum members,

we are developing a I2C to 1-wire interface board with one I2C bus and for three 1-wire segments. Because the 1-wire master DS2484 has a fixed I2C address, can we use it together with the I2C address translator LTC4317 ? That means for one DS2484 the I2C is connected direct, and the other 2 DS2484 via your double I2C address translator LTC4317. Is there expierence with such a solution?
 
Because we need the advance capabilities of the DS2484 we can't use a DS2482-100 as 1w master, where we can select different addresses.
 
Man thanks in advance for your help and answers!
 
Regards,
 
Ralf

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.