Post Go back to editing

What Are the Consequences of Power Interruption During the Programming Process of DS28E07?

Category: Datasheet/Specs
Product Number: DS28E07
From the datasheet, I understand that after sending the "Copy Scratchpad" command to the DS28E07, the chip will enter the programming state, which lasts for a maximum of 12ms. I would like to ask: what specific internal steps does the chip execute during this period, and what consequences will occur if there is a power interruption midway?
In my own tests, I observed that during the programming state, the chip first erases the original data. Notably, it erases 16 bytes at a time to the value of 8'hFF. For example:
  • If I edit bytes 0~7, the entire range of bytes 0~15 will be erased.
  • If I edit bytes 24~31, the entire range of bytes 16~31 will be erased.
After this erasure step, the chip proceeds to write the new data. Given this process, if a power interruption happens midway, will it result in scenarios such as:
  1. The data being erased but not rewritten, leaving all relevant bytes as FF?
  2. Corrupted (garbled) data due to incomplete programming?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.