Post Go back to editing

Help: Reading ADAU1797A over SPI with Aardvark (Control Center)

Category: Hardware
Product Number: adau1797a

I’m running a custom algorithm on the ADAU1797A and want to build a tuning tool that updates parameters at runtime.

Setup

  • Hardware: ADAU1797A, Aardvark adapter on SPI (J1).

  • Firmware: I created a dedicated memory region in the linker script so the tuning data lives at a fixed address. I can read/write this region fine with the debugger.

Issue

  • Using the Aardvark + Total Phase Control Center to read that address over SPI returns all zeros.

What I’ve tried

Request


Could someone share a minimal example of performing SPI reads from the ADAU1797A using an Aardvark, ideally in C# (Aardvark API) or a Control Center batch script? A snippet that:

  1. switches the ADAU1797A from I²C to SPI,

  2. performs a register/memory read (including the correct address format and R/W bit handling),

  3. shows expected SPI mode, clock polarity/phase, bit order, and chip-select behavior

…would be hugely appreciated.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.