Post Go back to editing

Enquiry Regarding the Wakeup and Sleep Pins of the DS28E17 1-Wire IC

Contains AI Generated Content
Category: Hardware
Product Number: DS28E17

Dear Analog Devices Team,

I am currently working on a project that requires a 1-Wire peripheral for communication. The device is intended to function as a 1-Wire slave. A sensor is connected to this slave device, and the slave will transmit the sensor data to the master device over the 1-Wire interface.

I have referred to the EVM schematic of the DS28E17.

According to the schematic provided in the EVM datasheet, the WAKEUP pin is connected to the 1W pin through a 0-ohm resistor, and the SLEEP_N pin is pulled up to 3.3V through a 3.3kΩ resistor.

I have the following questions:

  1. Can the WAKEUP pin be pulled up to VDD permanently? (I would like to keep the device awake at all times.)
  2. Is it necessary to put the device into sleep mode? 

Thank you for your support.