KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
DS2401
Recommended for New Designs
The DS2401 enhanced Silicon Serial Number is a low-cost, electronic registration number that provides an absolutely unique identity which can be determined...
Datasheet
DS2401 on Analog.com
Looking for clarification on the package thermal resistance for DS2401. I am specifically interested in the max junction temperature and junction-to-case resistance.
The datasheet only provided ambient ratings for the part in the absolute maximum ratings section.
Operating Temperature Range: -40°C to +85°C
Storage Temperature Range: -55°C to +125°C
The package I need information on is part number DS2401P+.
Package Type: 6 TSOC
Outline 21-0382
If any of information is not available, similar information would be helpful (such as the junction-to-ambient, similar part numbers, etc.).