Post Go back to editing

3,3V Programming MAX78000

Category: Hardware
Product Number: MAX78000

Hello,

I want to program the MAX78000 through an 3,3V device. The Eval Board works only with 1,8V for programming.

I know that there are two I/O Voltages at MAX78000 1,8V and 3,3V.

Is ist possible to program MAX78000 by default with 3,3V voltage level or is there any way to start MAX78000 after Reset with support for 3,3V at the programming pins?

Thanks for your help