TS201 S/W exception interrupts

Hi

I am trying to enable software exception interrupts on a TS201 processor, without success.

I specifically want interrupts on floating-point errors (e.g. div-by-zero).

I enabled global interrupts, unmasked the bits in the XSTAT/YSTAT registers, and unmasked the bit in the SQCTL register, but my ISR is still never executes.

The following is an extract from my test code:

int swErrCnt = 0;

void SWerrorISR(int signal) { swErrCnt++; }

void TestSWinterrupt(void)
{
  __builtin_sysreg_write(__SQCTLST, 0x0004);  // Global interrupt enable  
  interrupt(SIGSW, SWerrorISR);  // Register interrupt handler
  //Unmask S/W interrupts:
  asm("R0 = STAT;;");
  asm("R1 = 0x700000;;"); //IVEN (invalid floating-point), OEN (overflow), UEN (underflow) 
  asm("R0 = R0 or R1;;");
  asm("STAT = R0;;");  
  __builtin_sysreg_write(__SQCTLST, SQCTL_SW);  // Unmask S/W exception interrupts in SQCTL register.
  // Force floating-point error
  volatile float aa = 1.0, bb = 0.0, cc;
  cc = aa/bb;  // Divide by zero
  printf("S/W IRQ count: %d", swErrCnt)
}

Any help will be appreciated!

Thanks

Thinus Viljoen

Parents Reply Children